Webinar:
How to Select the Right Connector or Interconnect for Harsh Environments
This webinar was recorded and is avalaible on our on-demand page.
Selecting the correct connector or interconnect system is key to avoiding costly failures, unplanned downtime, product recalls, and potential reputational damage. In this expert-led webinar, you will gain valuable insights into connector selection, rugged design enhancements, and real-world applications that extend far beyond the automotive industry.
Whether you work in mining, transportation, energy, or industrial automation, understanding how to choose and apply harsh-environment connectors can drastically improve your design’s reliability and lifecycle
Tune in and learn:
- How the right interconnect choices can safeguard your designs from costly failures, unexpected downtime, and reputational risks, especially in harsh or
high-demand environments. - Which design parameters and connector features truly matter when long-term reliability and performance are non-negotiable.
- How Molex’s automotive-grade solutions go beyond automotive, with real-world examples and market insights showing their impact across industries like industrial automation, commercial vehicles, and medical.
This webinar was recorded and is avalaible on our on-demand page.
Recording
Question & Answers
1. Is the panel-mount version available in metal housing?
MX150 does not have metal housing. Metal shrouded connectors are often found in applications such as industrial or rail. An example is Molex’s Heavy-Duty Connector family such as the GWconnect Modular System.
2. What are the recommended methods to protect solder connections in mil-spec cable connectors with many contacts from shorting?
Ensure proper strain relief. Solder joints alone must not carry mechanical load.
A backshell with an integrated strain relief clamp or grommet can prevent pulling force from reaching soldered connections.
Prevent cold solder joints, solder bridging, or exposed conductor near other pins.
Use individual heat shrink tubes over each soldered connection to insulate and protect.
For connectors with solder cups, ensure wires are fully inserted and solder fillets are clean, with no stray strands.
We recommend considering AirBorn, a Molex company, as the supplier for pre-assembled wires. Our crimped wires provide a more robust integration into each insulator. Furthermore, pre-terminated wires from AirBorn can be enhanced with pre-potting and various epoxy materials for superior performance.
By offering both pre-installed wires and complete cable harness solutions, we enable customers to simplify their designs, reduce the need for subcontractors, and consolidate sourcing. Our expertise minimizes the risk of shorting and ensures exceptional integration.
3. Can the gasket be made of silicone or fluorosilicone with oriented wire mesh for IP and EMI protection?
The blue gasket that was shown on the MX150 panel mount connector is manufactured from Silicone. This seal is for ingress protection only and does not provide EMI protection.
4. What is the best sealed connector system for mounting a receptacle to a metal enclosure, ensuring proper contact between the connector body and the housing?
- The cable used is shielded (e.g., CAN bus or multi-core signal cable with ~10 wires).
- The shield should terminate at the housing connector.
Molex M12 connectors accommodate shielded cable and have panel mount versions available. The shielding is transferred to the receptacle via the M12 cap nut and can thus be connected to the housing. The Molex Ultra-Lock is rated to IP69 when mated.
5. Do the locking mechanisms also help protect contact patches from wear caused by vibration?
Contact wear due to vibration usually results from micro-movements that cause fretting corrosion or mechanical degradation at the contact surfaces. By holding terminals securely in place, TPA and ISL reduce these micro-movements. While they do not directly eliminate wear, they reduce the mechanical causes that contribute to wear and contact degradation
6. Does Mizu-P25 come with silver plating? What is the current rating for that version?
Mizu-P25 is available in 2 different versions; Standard and Miniature. Both have tin plated terminals and are rated to 250v. The standard version is capable of 3A, the Miniature version can carry up to 4A depending on cable type.
7. Can you comment on how gold plating thickness affects corrosion robustness?
Thicker gold plating improves corrosion resistance by reducing porosity and protecting contact surfaces in harsh environments. Molex specifies plating thickness based on application needs to ensure reliability without compromising solderability or cost. Excessive thickness can lead to issues like gold embrittlement, so standards like ASTM B488 guide optimal use.
8. Do you offer connectors with 0.8 µm electroplated gold over nickel?
Yes, Molex offers connectors with 0.8 µm electroplated gold over nickel. Product-specific plating details can be filtered on Molex.com by material and minimum thickness to match your application needs. This allows engineers to quickly identify suitable parts for demanding environments. Molex designs plating options to balance performance, durability, and cost across a wide range of applications.
9. All highlighted products seemed to be designed for automotive applications. Are they also suitable for other markets?
Yes, they are. While these connectors are designed to meet stringent automotive standards, their robustness makes them suitable for other demanding markets such as industrial automation, medical devices, and consumer electronics. When electrical, mechanical, and environmental requirements are clearly defined, Molex connectors can offer reliable solutions across a wide range of applications. Product specifications and approvals help guide cross-industry use.
10. The stAK50h looks like a flexible solution for unsealed wire-to-box applications. What does Molex offer in the sealed range?
Molex offers several sealed wire-to-device connector families, including MX150, CMC/CMX, Compactus, and MX123, all designed for harsh environments. For sealed data transmission, HSAL II is available. These solutions meet automotive-grade sealing requirements and are also suitable for industrial and off-highway applications. Detailed specifications and sealing ratings can be found on Molex.com.
11. For the stAK50h connector, is there guidance available to help identify the best bay combination for specific application needs?
Yes, there is a stAK50h configurator available on Molex.com. You can select the number of pins needed for each terminal size, and the tool will suggest compatible bay combinations. This helps ensure the connector layout matches your application’s electrical and mechanical requirements. Molex also provides technical documentation to support design decisions.
Host & Speaker(s)

Host
Mark Patrick
Technical Content Director EMEA,
Mouser Electronics Inc.
As Mouser Electronics´ Director of Technical Content for EMEA, Mark is responsible for creating and circulating technical content within the region. Before leading Technical Content, Mark was part of Mouser’s EMEA Supplier Marketing team and played a vital role in establishing and developing relationships with key manufacturing partners. Mark’s previous experience encompasses active engineering roles, technical support, semiconductor technical sales, and various marketing positions. A “hands-on” engineer at heart, Mark holds a first-class Honors Degree in Electronics Engineering from Coventry University.

Speaker
Ian Vanner
Business Development Manager – Distribution Transportation Innovative Solutions, Molex
Ian began his career as a Mechatronic Design Engineer, bringing a strong foundation in mechanical and electronic systems integration. Since 2001, he has been deeply involved in Automotive and Commercial Vehicle applications. Currently, Ian plays a key role in supporting Molex’s distribution channel, where he collaborates closely with partners and customers to solve complex engineering challenges. His focus is on delivering rugged and reliable connectivity solutions that meet the evolving needs of the transportation industry. Ian is passionate about innovation, customer success, and leveraging technology to drive performance and durability in harsh conditions.
Featured products
Don't miss anything - Register now for the Mouser News & Events Newsletter »